Datasheet is clear - The range can be set to +5 V, +10 V, +10.8 V, ±5 V, ±10 V, or ±10.8 V.
But can the range be different per channel?
If yes - so there are no restrictions apart from the fact that the supply voltage should be sufficient for all selected ranges (Highest one). Right?
The selection "BIN/2sComp" is obviously common for all channels.
Thanks
Edit Notes
added note about BIN/2sComp[edited by: larsen at 8:26 PM (GMT -4) on 15 Aug 2021]