Post Go back to editing

AD5175 Potentiometer Reset

Thread Summary

The user is experiencing an issue with the AD5175 potentiometer where the wiper resets to the middle position after 20 minutes, despite no power cycle. The final answer suggests checking the RESET pin, which should not be tied directly to VCC. Additional troubleshooting includes monitoring all signals and ensuring a 1uF capacitor is connected between EXT_CAP and GND. The user confirmed the capacitor is connected but still faces the issue, and the engineer recommends sharing a circuit diagram for further analysis.
AI Generated Content

Hi All

I am trying to communicate the AD5175 Potentiometer. Once  set the Resistor to 1Kohm using the Microcontroller Program after 20 Minutes the Potentiometer go to the Mid values .I am get confused without Power OFF & ON still Potentiometer go to the Mid value.

Thanks

Jay