Post Go back to editing

DAC8420 +5V operation. Outputs don't go lower than 600mV. Damaged device?

I'm testing a DAC8420FPZ (PDIP).

I run a loop where I output value 0 to 4095 to make a sawtooth waveform.

But the waveform is clipped at 600mV. It can't go lower than 600mV.

Is the device damaged?

I have connected:

GND = ground

CLR = ground

VDD = +5V

VREFHI = +2.5V

VREFLO = ground

VSS = ground

Parents Reply Children