Hello,
How often is the value of the Iout Fault bit updated?
How long does the Iout Fault bit hold the value 1?
When a disconnection occurs during operation, the /FAULT signal is detected and the Iout Fault in the STATUS REGISTER is read, but sometimes the Iout Fault bit is 0.
It takes time to read the register value because the process of SPI communication 1Mbps (AD5410 x 8 daisy-chain connection) is performed after /FAULT signal is detected.
It is assumed that the /FAULT occurrence register (Iout Fault=1) could not be read because Iout Fault returns to 0 during the process described above.
This is the reason why I asked this question.
Regards,
Kazu