Post Go back to editing

LTC1666 - Vref - input resistor

Hello fellows, I'm building my own DAC Eval Board and Im wondering to know ..

  1. if the External Vref  (suggested 2.5v) Can be set in a higher value?, like 5v. I only read about, adjusting Irefin current by resistor avoiding to source more than 10mA, but nothing about the Vref max limits values (May be, not exceed the sourcing values? +/- 5v). The higher Vref values in the DAC, the higher voltage range per counts (better for noise issues)
  2. About the DAC inputs, Is it necessary to put 22ohms resistor between the FPGA ouput and the DAC input ports? (I'm interfacing a Cyclone V with the DAC) Datasheet suggest to use a resistor bank in Application Information Section - Suggested Evaluation Circuit.

Thanks in advance!



l
[edited by: HernArg at 4:12 PM (GMT -4) on 26 Apr 2021]