Post Go back to editing

Programming LTC2636

I tried to use LTC2636, so far no luck

First I output 0x7000 via SSI, to set it up to use external reference (I can confirm 0x7000 on CS, SCK and SDI with logic analyzer)

Then I output 0x0080 via SSI, to write 0x80 to register 0

finally I output 0x0100, to update the dac, but i got nothing on VoutA

Did I miss something? Thanks for your time

Below the schematic

Parents
  • Hi,

    What variant of the LTC2636 are you using? (-12, -10, -8) You should be sending out 24 clock edges for a valid transaction. Can you send a scope shot of your CS, SCK, and SDI signals?

    What voltage are you supplying on the REF pin? Can you confirm if that is the actual voltage on the pin?

    Best regards,

    Ian

Reply
  • Hi,

    What variant of the LTC2636 are you using? (-12, -10, -8) You should be sending out 24 clock edges for a valid transaction. Can you send a scope shot of your CS, SCK, and SDI signals?

    What voltage are you supplying on the REF pin? Can you confirm if that is the actual voltage on the pin?

    Best regards,

    Ian

Children