50-TP memory of AD5270

Hi,

i was wondering, if its possible to delete or overwrite the 50-tp memory of the AD5270.

Thanks in advance

Top Replies

Parents
  • 0
    •  Analog Employees 
    on Feb 8, 2021 12:20 PM

    Yes, the TP-memory can be overwritten upto 50 times.

    The AD5270/AD5271 contain an array of 50-TP programmable memory registers, which allow the wiper position to be programmed up to 50 times. Table 13 shows the memory map. When the desired wiper position is determined, the user can load the serial data input register with Command 3 (see Table 11) which stores the wiper position data in a 50-TP memory register. The first address to be programmed is Location 0x01 (see Table 13); the AD5270/AD5271 increments the 50-TP memory address for each subsequent program until the memory is full.

Reply
  • 0
    •  Analog Employees 
    on Feb 8, 2021 12:20 PM

    Yes, the TP-memory can be overwritten upto 50 times.

    The AD5270/AD5271 contain an array of 50-TP programmable memory registers, which allow the wiper position to be programmed up to 50 times. Table 13 shows the memory map. When the desired wiper position is determined, the user can load the serial data input register with Command 3 (see Table 11) which stores the wiper position data in a 50-TP memory register. The first address to be programmed is Location 0x01 (see Table 13); the AD5270/AD5271 increments the 50-TP memory address for each subsequent program until the memory is full.

Children