Hi,
May I know what type of application will you use the AD5370 for? Is there a tight spec on the write time? In the case of AD5370, SYNC is required after every 24clock cycles to ensure that the data…
May I know what type of application will you use the AD5370 for? Is there a tight spec on the write time? In the case of AD5370, SYNC is required after every 24clock cycles to ensure that the data won't be corrupted and written to the correct register.
writing a frame for 40channels would require 39 sync pulses since the last sync should remain high if there are no other data to be sent in the serial bus.
Having two registers allows the holding of 2 sets of output settings for each channel. Let me clear up that each channel can be configured as to which input register will it take its data from. This could be useful in applications where there would be 2 sets of output values. Switching to the second set of output data would take less number of SPI word transactions compared to writing to all 40 channels individually.
Let me know if I have answered your questions.
Best regards
Ian