EVAL-AD5761RSDZ

Hi,

I am currently working with the EVAL-AD5761RSDZ. I am trying to control the DAC with a Python script running on a Raspberry Pi.

As far as I know I have to write to the control register after powering up. By sending 0x04 04 11 the DAC should be configured to the output range from 0V to 10V.  Then I can use the write and update command, 0x03 ff ff, to set the voltage output to its maximum. However, the output remains unchanged at 0V. I have also tried to start with a "software full reset" command, but the result is the same. While checking the connections of the DAC I couldn't find any issues. The signal on the MOSI line goes into the chip, as well as the CLK signal, the sync signal and the provided power.

Do you have any idea what I could be doing wrong or how I can solve this problem?


Parents
  • 0
    •  Analog Employees 
    •  Super User 
    on Nov 3, 2020 3:12 AM

    Hi, 

    Have you checked the jumper settings on the EVAL-AD761RSDZ? What's your setting for LK1 to LK4?

    How about the supply connectors J1, J2, J5? What's your voltage setting on these pins?

    Can you also show an OSC capture of your SPI transactions? 

    Are you using internal reference, external on-board reference, or external reference?

    Hope you can answer the above queries so I can helpo you out.

    Best regards,

    Ian

Reply
  • 0
    •  Analog Employees 
    •  Super User 
    on Nov 3, 2020 3:12 AM

    Hi, 

    Have you checked the jumper settings on the EVAL-AD761RSDZ? What's your setting for LK1 to LK4?

    How about the supply connectors J1, J2, J5? What's your voltage setting on these pins?

    Can you also show an OSC capture of your SPI transactions? 

    Are you using internal reference, external on-board reference, or external reference?

    Hope you can answer the above queries so I can helpo you out.

    Best regards,

    Ian

Children
  • Hi,

    Yes I did checked the jumper settings, but I feel like that this is not the cause of my Problem. The Links of LK2 and LK14 are removed. On the other hand, the Links of LK7 and LK8 are inserted and the Links of LK_AVDD, LK_AVSS, LKDVCC, LK_REF, LK_VOUT+, LK_VOUT- are conected to B.

    Power is supplied via the  PVIN_3V-15V connector. The input voltage and messured voltage on these conectors is 10V.  The voltage messured on the Vss Pin is -11V and on the VDD Pin 21V. The Voltage at the DVcc Pin lays around 2.3V.

    I am using an internal reference selected by position B of the LK_REF Pins.

    This is the Date send to initilize the DAC.

    And this is the write and update command.

    The yellow signal is the clock signal and the green signal is the MOSI signal.

    I hope that this answers your questions. If not, please let me know what else you need.

    Best regards,

    Nils

  • 0
    •  Analog Employees 
    •  Super User 
    on Nov 6, 2020 3:58 AM in reply to Nils

    Hi Nils, 

    I don't have an eval board with me right now. I'm curious as to why the DVcc is around 2.3V. I looked through the schematic and found that with your current jumper settings, there is no actual supply going into the DVCC pin. I'm thinking the LK_DVCC pin should be on pos A, that will give a good 5V into the DVCC pin.

    I also noticed that the MOSI is set at the falling clock edges. This will pose a problem as the AD5761R also reads the data on the falling clock edge. In this case, we need to make sure that the data is already valid on the falling edge so it would be better for the MOSI to set date on the rising edge. You can refer to the Serial Interface section of the datasheet. 

    Let me know if the above works. 

    Best regards,

    Ian

  • Hello Ian,

    I changed the position of the LK_DVCC pin with the result that 5V were measured at the DVCC pin.

    Regarding the operating modes for the MOSI line I have two options. Option one is selected in the last snapshots and the second mode is selected in this picture.

    Unfortunately these adjustments did not solve my problem. I still have a VOUT of 0V. Do you have any other suggestions what I can try?

    Thank you very much for your efforts, I really appreciate it.

    Best regards,

    Nils

  • 0
    •  Analog Employees 
    •  Super User 
    on Nov 10, 2020 4:00 AM in reply to Nils

    Hi Nils, 

    Hardware setup and SPI mode should be ok now. 

    I'm reviewing your SPI commands, 

    0x04 04 11 - You should enable the internal reference (IRO) bit, it should be 0x04 04 31.

    The power-up voltage (PV) is set to 10: full scale at startup. so you might not need the 2nd spi transaction. 

    Let me know if this works.

    Best regards,

    Ian

  • Hi Ian,

    I did what you said, but I still get 0V as output. Are you sure about the SPI command? The datasheet says that DB5 should be 0 for all control register commands.

    I also checked my hardware setup and changed the LK_REF pin to position B to enable on-board reference. But there is still no change in the output value.

    Do you have any other suggestions what might help?

    Best regards,

    Nils