The AD5696RBRUZ data sheet only mentions a sink current of 3 mA. We need to go from a 2.1 kOhm pull up at +5VDC(2.3 mA) to a 1kOhm pull up at +5VDC (5 mA) since we have too many devices on the I2C buss. Can the AD5696RBRUZ sink the 5 mA on the SDA line? The device is a slave so it is not driving the SDL at all so that is not an issue.