SPI Communication with EVAL AD5755-1

Hello, I'm trying to communicate with an AD5755-1 using the EVAL board.  I've hooked up my SPI connections to the appropriate pins, but I can't replicate the activity when I use the EVAL board software.  I'm using an arduino with 

SPI.beginTransaction( SPISettings( 500000, MSBFIRST, SPI_MODE3 ) );

Here is my current input/output streams.

Starting
Chip: 00 CS_PIN:25
Software Reset
Sending: {1C, 85, 55};
Received: {E0, 80, 0};
DCDC register write
Sending: {1C, 60, 7};
Received: {0, 80, 0};
Main Control Register Write (16mA)
Sending: {1C, 22, 0};
Received: {0, 80, 0};
read main control register (0200 expected)
Sending: {99, 0, 0};
Received: {0, 0, 0};
Main Control Register Write (8mA)
Sending: {1C, 22, 40};
Received: {0, 80, 0};
read main control register (0000 expected)
Sending: {99, 0, 0};
Received: {0, 0, 0};
read main control register (0000 expected)
Sending: {99, 0, 0};
Received: {0, 0, 0};
gain register
Read Gain Register
Sending: {88, 0, 0};
Received: {0, 0, 0};
NOP CMD
Sending: {1C, E0, 0};
Received: {0, 80, 0};

Please advise on how to address this communication issue.  I've tried a bunch of different things, but I just can't replicate the EVAL software results.  Is there a problem in my setup protocols?

Parents
  • 0
    •  Analog Employees 
    •  Super User 
    on Sep 25, 2020 6:31 AM

    Hi, 

    Can you give a scope capture of your digital transaction?

    Can you also give a simple i/f diagram of your controller and the eval board?

    Not very familiar with arduino spi_mode3, but ad5755-1 has a serial interfacing diagrams in the datasheet. not sure if generic SPI protocols would work.

    Best regards,

    Ian

  • Thank you for getting back to me.

    I've attached scope data below.

    Blue = SDIN

    Yellow = SCLK

    Green = SDO

    Red = SYNC

    I believe the timings are fine in accordance with Table 3 and Figure 4 of the AD5755 Revision E documentation.

    As for the diagram, It's pretty straightforward as described below.  There are 6 total connections:

    Arduino - 5755 Eval Board (pins 1-6 on Figure 2 and Table 3

    3v3 - DvDD

    AGND - DGND

    SCLK - SCLK

    MOSI - SDIN

    MISO - SDO

    PIN 25 - SYNC

  • 0
    •  Analog Employees 
    •  Super User 
    on Sep 29, 2020 3:31 AM in reply to Benjamin.G

    Hi,

    Looks like the timing is indeed OK.

    About the connections, If there is space on your Arduino, try and assign a pull-up or a default high IO for the RESETB pin.

    I'm curious as to how your IO stream works, for example:

    Software Reset
    Sending: {1C, 85, 55};
    Received: {E0, 80, 0};

    Is the "received" data here, the SDO output on the same frame as the "Sending" data? I'm assuming this is the case.

    About the sequence below, it is recommended that the read transaction is followed by either another read transaction or a NOP. Your readback data is clocked out of the SDO output on this next transaction. This also means that a write command should follow either another write command or a NOP. 

    Main Control Register Write (16mA)
    Sending: {1C, 22, 0};
    Received: {0, 80, 0};
    read main control register (0200 expected)
    Sending: {99, 0, 0};
    Received: {0, 0, 0};
    Main Control Register Write (8mA)
    Sending: {1C, 22, 40};
    Received: {0, 80, 0};

    This sequence below is correct, readback on the DAC register and the received data during NOP should be the DAC register data but should've been 0x0 (default value). Please try to fix the sequence for the other transactions and let's see if it works. 

    Best regards,

    Ian

Reply
  • 0
    •  Analog Employees 
    •  Super User 
    on Sep 29, 2020 3:31 AM in reply to Benjamin.G

    Hi,

    Looks like the timing is indeed OK.

    About the connections, If there is space on your Arduino, try and assign a pull-up or a default high IO for the RESETB pin.

    I'm curious as to how your IO stream works, for example:

    Software Reset
    Sending: {1C, 85, 55};
    Received: {E0, 80, 0};

    Is the "received" data here, the SDO output on the same frame as the "Sending" data? I'm assuming this is the case.

    About the sequence below, it is recommended that the read transaction is followed by either another read transaction or a NOP. Your readback data is clocked out of the SDO output on this next transaction. This also means that a write command should follow either another write command or a NOP. 

    Main Control Register Write (16mA)
    Sending: {1C, 22, 0};
    Received: {0, 80, 0};
    read main control register (0200 expected)
    Sending: {99, 0, 0};
    Received: {0, 0, 0};
    Main Control Register Write (8mA)
    Sending: {1C, 22, 40};
    Received: {0, 80, 0};

    This sequence below is correct, readback on the DAC register and the received data during NOP should be the DAC register data but should've been 0x0 (default value). Please try to fix the sequence for the other transactions and let's see if it works. 

    Best regards,

    Ian

Children
  • Ian,

    I've added the following connections.  These are static for the duration of the tests, but can be controlled.

    RESET is pulled to 3v3,

    LDAC to 3v3, and

    CLEAR to 0v

    This has not changed the initial results.

    Is the "received" data here, the SDO output on the same frame as the "Sending" data? I'm assuming this is the case.

    You have the correct interpretation of what is going on.  So if a read command was not the previous command, this data would not be used.  It's included for posterity and debugging.

    Please try to fix the sequence for the other transactions and let's see if it works. 

    I think this is the sequence you wanted.  I made sure to include NOP commands after every read command.

    Software Reset
    Sending: {1C, 85, 55};
    Received: {E0, 80, 0};
    DCDC register write
    Sending: {1C, 60, 7};
    Received: {0, 80, 0};
    Main Control Register Write (16mA)
    Sending: {1C, 22, 0};
    Received: {0, 80, 0};
    read main control register (0200 expected)
    Sending: {99, 0, 0};
    Received: {0, 0, 0};
    NOP CMD
    Sending: {1C, E0, 0};
    Received: {0, 80, 0};
    Main Control Register Write (8mA)
    Sending: {1C, 22, 40};
    Received: {0, 80, 0};
    read main control register (0000 expected)
    Sending: {99, 0, 0};
    Received: {0, 0, 0};
    NOP CMD
    Sending: {1C, E0, 0};
    Received: {0, 80, 0};
    gain register
    Read Gain Register
    Sending: {88, 0, 0};
    Received: {0, 0, 0};
    NOP CMD
    Sending: {1C, E0, 0};
    Received: {0, 80, 0};

    What else could it be? 

    Thanks in advance,

    -Benjamin

  • +1
    •  Analog Employees 
    •  Super User 
    on Sep 30, 2020 5:21 AM in reply to Benjamin.G

    Hi Benjamin, 

    I'm comparing your waveforms from my previous tests. I noticed you are clocking out data on the falling edge from your Arduino. AD5755-1 also clock-in on the falling edge. This might cause some mismatch with the data. Can you config your controller to clock out data on the rising edge, so that when data reaches the device, it should be in a stable state at the following falling edge? Let me know if this works. 

  • Ian,

    This did the trick! Using an Arduino with SPI_MODE2 (below) gives me proper behavior.  I can now start building my firmware.  Thank you!

    -Benjamin

    Mode Clock Polarity (CPOL) Clock Phase (CPHA) Output Edge Data Capture
    SPI_MODE0 0 0 Falling Rising
    SPI_MODE1 0 1 Rising Falling
    SPI_MODE2 1 0 Rising Falling
    SPI_MODE3 1 1 Falling Rising
  • 0
    •  Analog Employees 
    •  Super User 
    on Oct 16, 2020 6:32 AM in reply to Benjamin.G

    Hi Benjamin,

    That's great to hear! This is a common occurrence in serial communications; clock timing and data out. In case there are other devices in your serial interface, be sure to check if they are compatible with respect to this serial mode timing. 

    Best regards,

    Ian