Post Go back to editing

DAC8412 Analog crosstalk

Hi.

Please tell me how parameter "Analog crosstalk" in DAC8412 measured like because in datasheet value is 72 dB.

This is the glitch impulse transferred to the output of one DAC due to a change in the output of another DAC. It is measured by loading one of the input registers with a full-scale code change (all 0s to all 1s and vice versa) while keeping  high. Then pulse LDAC low and monitor the output of the DAC whose digital code was not changed. The area of the glitch is expressed in nV secs.

or

It is defined as the ratio of the signal level on one channel while the opposite channel is held at idle level. In other words , this is a measure of crosstalk between adjacent channels. It can be measured by evaluating distortion on the idle channel when the opposite channel has data present.

Thanks.

Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.