What are the differences between the AD5060, AD5061, AD5062 and AD5063 low voltage single channel 16-bit resolution DACs?
What are the differences between the AD5060, AD5061, AD5062 and AD5063 low voltage single channel 16-bit resolution DACs?
All these DAC are 16-bit resolution single channel DACs are are monotonic.
AD5060: Buffered output, +/- 1 LSB INL in 8-SOT 23
AD5061: Buffered output, +/- 4 LSB INL in 8-SOT 23
AD5062: Unbuffered output, low TUE, +/- 1 LSB INL in 8-SOT 23
AD5063: Buffered output,+/- 1 LSB INL in 10-MSOP*
*Allows access to the internal scaling and feedback resistors of the DAC and is useful for bipolar operation.