Hi ,
As mentioned in the datasheet of AD5755 ,
The Transient Voltage protection circuit for Current Output following components are required :-
External power diodes , transient voltage suppressors & surge current limiting resistor , as shown in Figure 84 of Datasheet .
->What are the recommended power ratings and part no. of the above components ?
Also In case of Voltage outputs , the recommended protection circuit must have following components as per Application note CN-6005 :-
A TVS diode , Non-Conductive ceremic ferrite bead , and power diodes.
-> What are the recommanded part no. of the above components ?
Can we use a TVS diode of Vbr 15V ?
Regards !!
VAV