Post Go back to editing

Output Protection Circuit for AD5755 ?

Hi ,

As mentioned in the datasheet of AD5755 ,

The Transient Voltage protection circuit for Current Output following components are required :-

External power diodes , transient voltage suppressors & surge current limiting resistor , as shown in Figure 84 of Datasheet .

->What are the recommended power ratings and part no. of the above components ?

Also In case of Voltage outputs , the recommended protection circuit must have following components as per Application note CN-6005 :-

A TVS diode , Non-Conductive ceremic ferrite bead , and power diodes.

-> What are the recommanded part no. of the above components ?

Can we use a TVS diode of  Vbr 15V ?

Regards !!

VAV