I am using AD5752R in 0-10V operation. But its getting configured only to 0-5V range. Wat may be the reason?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
I am using AD5752R in 0-10V operation. But its getting configured only to 0-5V range. Wat may be the reason?
Hi arunkrishnank,
It seems that the part is not being configured to change the default output range of +5V to a +10V range. Please make sure that the DVCC is brought high before any of the interface lines are powered. If this is not done the first write to the device may be ignored, and as you are configuring the output range on the first write this could be not taken into account.
Hi arunkrishnank,
It seems that the part is not being configured to change the default output range of +5V to a +10V range. Please make sure that the DVCC is brought high before any of the interface lines are powered. If this is not done the first write to the device may be ignored, and as you are configuring the output range on the first write this could be not taken into account.