AD5412 with I and V out on same pin

We are looking to use the AD5412 with I and V out going to the same pin.  I notice they call out using a buffer amplifier on the V+sense line in this case.  Our device has an input range of 12 to 30V which will be used to power the AD5412 as well the V+ and V- of the amplifier.  Can I use the OP07 recommended buffer amp in this case?  Thanks.

Parents
  • 0
    •  Analog Employees 
    on Dec 5, 2012 4:00 PM over 8 years ago

    Hi,

    The following part would suit your needs.

    The OP290 is a high performance micropower dual op amp that operates from a single supply of +1.6V to +36V or from dual supplies of ±0.8V to ±18V. Input voltage range includes the negative rail allowing the OP290 to accommodate input signals down to ground in single supply operation.

    Regards,

    Michael (PDA Applications)

Reply
  • 0
    •  Analog Employees 
    on Dec 5, 2012 4:00 PM over 8 years ago

    Hi,

    The following part would suit your needs.

    The OP290 is a high performance micropower dual op amp that operates from a single supply of +1.6V to +36V or from dual supplies of ±0.8V to ±18V. Input voltage range includes the negative rail allowing the OP290 to accommodate input signals down to ground in single supply operation.

    Regards,

    Michael (PDA Applications)

Children
No Data