Hi,
Im trying to use AD7397 for generating an voltage swing from -3V to +3V. I have made the bipolar connections as per the datasheet. The connections were as follows :
Vin= Vref= 3V
AGND = DGND = Ground
D0- D9 = High through Microcontroller
RS= SHDN = A/B = LDB= 3V
LAD = 0V
CS= Was changed high and low with a microcontroller.
This is not giving any output. Kindly suggest and correct.
I have attached the circuit for the same.