Two AD5116 + One SSM2306

Hi,

I am planning to use ADI push button in my volume control design.

I will use SSM2306 (Stereo Audio Amplifier) in this project, and I am wondering if I can use 2 AD5116 to do the volume control? Each AD5116 will be connected with Left or Right channel audio signal.

I also wonder if I can use a same combination of push buttons to control both AD5116 at the same time?

Is this solution workable?

I attach a simple circuit which I would like to design for my audio volume control, kindly advice me if that is workable.