Post Go back to editing

AD5791 - Driving a load of 1uF

Hi,

 

 

My design demands a setup as shown in attachment. The design doesn't demand a quick settling time. Also, it happens only once.

 

I need some clarifications related to that.

1. Is there any stability problems.

2. can it drive this load. (settling time is not a concern)

 

LTC1043 - It is a switched capacitor based voltage inverter. This inverter block has a switched capacitor of 1uF. The switching frequency is 250Hz.

There are buffers placed after this LTC1043, so no current is taken out from LTC1043.

 

 

Thanks,

Jebas.