Post Go back to editing

Is there a daisy-chainable high-precision (18+ bits) DAC

Hi,

I need to daisy-chain several AD7767 along with high-precision DACs in a way such that the DACs can be updated while reading data from the ADCs. It is a relatively large system with hundreds of ADCs/DACs. The daisy-chaining is necessary to meet my overall timing requirements.

I was thinking about using AD5791s, but then realized that they cannot be daisy chained. (The original datasheet showed a daisy-chaining mode.)

 

Is there any way to daisy-chain 5791s? Alternatively, is there a high-precision DAC with that can be daisy-chained with AD7767s (24-bit regs, similar timing, ...)?


Thanks!

Parents
  • Hi Mark,

    Thanks for your help!

    I'm sure that the daisy chaining mode for the AD57* DACs was removed for a good reason, i.e., that it just did not work. There are also other posts on this, e.g., http://ez.analog.com/message/122605#122605. I think it is safe to assume that this won't change in the foreseeable future.

    The AD760 is unfortunately not a good option for me. It has close to 13 dB higher noise floor, rather bad THD+N, and it's mode of operation would be hard to combine with the 24-bit AD7767.

    Best regards,

    Daniel

Reply
  • Hi Mark,

    Thanks for your help!

    I'm sure that the daisy chaining mode for the AD57* DACs was removed for a good reason, i.e., that it just did not work. There are also other posts on this, e.g., http://ez.analog.com/message/122605#122605. I think it is safe to assume that this won't change in the foreseeable future.

    The AD760 is unfortunately not a good option for me. It has close to 13 dB higher noise floor, rather bad THD+N, and it's mode of operation would be hard to combine with the 24-bit AD7767.

    Best regards,

    Daniel

Children
No Data