Dear Sir:
May I use AD5754R and AD5752R for Daisy-Chain function of 6 channel DAC output? BTW, In daisy-chain mode, May I has been pull low for LDAC pin?
Best Regard
Jason
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
Dear Sir:
May I use AD5754R and AD5752R for Daisy-Chain function of 6 channel DAC output? BTW, In daisy-chain mode, May I has been pull low for LDAC pin?
Best Regard
Jason
Hi Jason,
I see no problem in using the two parts in daisy chain mode to implement a 6 channel DAC output. Keep in mind on how the daisy chaining works. Please refer to the Daisy-Chain Operation section in the datasheet for detailed information on daisy-chaining SPI devices.
When operating in daisy chain mode, all your devices are connected to a single SCLK, SYNC, and LDAC. Yes, you may but remember that when LDAC is tied permanently low, the addressed DAC register is updated on the rising edge of SYNC.
If you have any other questions, please do not hesitate to ask.
Regards,
Mark