AD5752 SPI Issue

Hello,

 

I have connected an AD5752 to an SPI bus in which there are a number of devices, for example an EEPROM. When the DAC is not connected, everything works fine, but when I connect it, I just get 0s every time I read data from the EEPROM. I am keeping the AD5752 SYNC signal high, but its SDO line is always low, so I guess that is the reason why I am just reading 0s. I am not using a daisy chain by the way.

 

Is the AD5752 is sending data (zeros from its internal registers) because of the clock pulses even though SYNC is kept high?

 

Thanks in advance!

 

Javi

Parents Reply Children
No Data