The datasheet of the AD5621 states the following offset error range:
typical value +/- 0.063 mV
maximum +/- 10 mV
As this is a very broad range I'd like to know under what conditions we have to
expect the maximum value.
In our application we use the DAC output as a kind of reference voltage.
+/-0.5mV offset would be acceptable.
The ambient temperature range is between 0°C and 60°C.
Who has experience with the AD5621 and can help on that topic?
Regards
Robert