Post Go back to editing

CONNECTION ERROR: AD5686R Evaluation Board was not detected

SDP board(EVAL-SDP-CS1Z) is detected by both software and the led on SDP board blinks. But error AD5686R Evaluation Board(EVAL-AD5686RSDZ) was not detected appears after that.

Tired 2 software;

 

1. AD5684R Evaluation Software( CD came with EVAL-AD5686RSDZ)

CONNECTION ERROR: AD5686R Evaluation Board was not detected.

Continuing in Simulation Mode.

 

2. AD5684R Evaluation Software V1.1(downloaded from website)

Prompt: ERROR CONNECTION

 

Using Windows 7 Home Premium SP1 64bit

Program installed in x86

 

Please advice what I should do or if you require more information.


Thank you!

Parents
  • Hi, Darren.

    The evaluation software emulates the SPI protocol through the use of the SPORT. The evaluation board's communication line is designed physically to connect to the SPORT pins of the EVAL-SDP-CB1Z.


    As you have mentioned you are using the EVAL-SDP-CS1Z. The SDP that you are using only have SPI, I2C/TWI, and GPIOs. It does not use SPORT.

    As indicated in the last paragraph on the first page of the UG-459:

    This evaluation board requires the EVAL-SDP-CB1Z board (SDP-B controller board), which is available for order on the Analog Devices website at www.analog.com.

    You would be able to use the evaluation board if you would use the EVAL-SDP-CB1Z.


    Regards,

    Mark

Reply
  • Hi, Darren.

    The evaluation software emulates the SPI protocol through the use of the SPORT. The evaluation board's communication line is designed physically to connect to the SPORT pins of the EVAL-SDP-CB1Z.


    As you have mentioned you are using the EVAL-SDP-CS1Z. The SDP that you are using only have SPI, I2C/TWI, and GPIOs. It does not use SPORT.

    As indicated in the last paragraph on the first page of the UG-459:

    This evaluation board requires the EVAL-SDP-CB1Z board (SDP-B controller board), which is available for order on the Analog Devices website at www.analog.com.

    You would be able to use the evaluation board if you would use the EVAL-SDP-CB1Z.


    Regards,

    Mark

Children
No Data