Post Go back to editing

CONNECTION ERROR: AD5686R Evaluation Board was not detected

SDP board(EVAL-SDP-CS1Z) is detected by both software and the led on SDP board blinks. But error AD5686R Evaluation Board(EVAL-AD5686RSDZ) was not detected appears after that.

Tired 2 software;

 

1. AD5684R Evaluation Software( CD came with EVAL-AD5686RSDZ)

CONNECTION ERROR: AD5686R Evaluation Board was not detected.

Continuing in Simulation Mode.

 

2. AD5684R Evaluation Software V1.1(downloaded from website)

Prompt: ERROR CONNECTION

 

Using Windows 7 Home Premium SP1 64bit

Program installed in x86

 

Please advice what I should do or if you require more information.


Thank you!

Parents
  • Error image show below in the picture

     

    Using the default jumper settings as follows

     

    Link Options Setup for SDP Control (Default)

    LK1 A

    LK2 A

    LK3 C

    LK4 B

    LK5 A

    LK6 B

     

    Only SDP board, 6V(J3) & AGND(J3) connected to EVAL-AD5686RSDZ

     

    J3 - 6 V board positive power supply is connected to power supply unit tuned to 6V with ground connected.

    J1 & J2 and all SPI pin not connected

Reply
  • Error image show below in the picture

     

    Using the default jumper settings as follows

     

    Link Options Setup for SDP Control (Default)

    LK1 A

    LK2 A

    LK3 C

    LK4 B

    LK5 A

    LK6 B

     

    Only SDP board, 6V(J3) & AGND(J3) connected to EVAL-AD5686RSDZ

     

    J3 - 6 V board positive power supply is connected to power supply unit tuned to 6V with ground connected.

    J1 & J2 and all SPI pin not connected

Children
No Data