Please teach internal VREF drive ability of AD5310BRMZ.
1.
Please teach the bandwidth to which Internal VREF can be output.
-Detail-
I think that I would like to connect the output of the VREF pin with external analogSW directly.
This analog switch switches GND to VREF.
A rectangular wave is made as a result.
2.
Please teach me Output Current Load Capability.
Output Current Load Capability has been described to data sheet P3 as 5mA.
Output Current Load Capability has been described to data sheet P17 as 50mA.
Which is correct?
Thank you .
Mark-san
Please refer to following URL.
AD5310R | datasheet and product info 10-Bit nanoDAC, SPI Interface and 2 ppm/°C On-Chip Reference | Analog Devices
I think that you confirmed not R product.
Thank you.
Regards,
Kotoo