Hello
I have some question about AD5412
As i see in the datasheet i can connect "Io" and "Vo". just need a buffer .
your recommended buffer is Dual Op-amp .
I don't need bipolar output range (-5~+5 ,-10~+10) because i don't have dual power supply on my board.
So i have to use single supply op-amp .
As you know most of the single supply opamp that have low offset are very expensive .
Could i use an ordinary (not low or ultra offset) like lm358 as buffer ?(i have tested in zero input out put is about 13 mv).
Could i Connect "io" to "Vo" even when i use Boost ?
Best regards