Parallel outputs of AD5737 for additional current drive?

I have a customer looking for a low cost, precision current source.  He wants a SPI interface and current up to 30mA.  Output voltage could range up to 16V.  His application does not require very high accuracy (1-2% is probably fine).  The AD5737 is a close fit using the 0-24 mA output range.  Can I parallel 2 of the outputs to get greater current drive?  If so, what is the easiest, safe way to do this?

 

Any other suggestions.  He has already considered CN0151.

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:01 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:01 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data