Post Go back to editing

Three electrode measurement for AD5933?

Thread Summary

The user is using the AD5933 for bioelectrical electrode impedance measurements in a three-electrode configuration. The issue was discontinuities in the Nyquist plot and large errors at low frequencies. The solution involved recalculating the MCLK for each frequency, ensuring the excitation signal was within the ADC range, and adjusting the high-pass filter cutoff frequency to 0.14 Hz. This resulted in continuous and more accurate impedance measurements.
AI Generated Content

Hi everybody,

 

we're using the AD5933 for bioelectrical electrode impedance measurements. Usually, the electrodes have to be immersed in a saline solution for measuring, and a 2 point measurement (Electrode to Reference electrode) adds unwanted potential offsets to the measurement. For a more accurate measurement, a technique using 3 electrodes is employed:

 

(Fig. 4 from this link)

Ralph Group : projects : Fabrication and characterization of graphene electrodes for electrochemistry experiments

Figure 4

Is there any way to connect the AD5933 in such an arrangement to measure impedance? Do you have any additional suggestions for performing such a measurement?

 

Thanks and Kindest Regards,

Oscar Cota

Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.