Post Go back to editing

Is AD5624 a possible replacement for AD5324?

We are looking at alternates for the AD5324 (mainly for cost reduction), and it seems that the AD5624 is a good candidate. Would the AD5624 be considered a very close replacement for the AD5324? The current DAC is used in a low speed correction loop with an external +5V reference, running at approximately 125kHz sample/update rate. Among the differences I see are pin mapping, and 24-bit DIN vs 16-bit DIN.

Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.