Post Go back to editing

Is AD5624 a possible replacement for AD5324?

We are looking at alternates for the AD5324 (mainly for cost reduction), and it seems that the AD5624 is a good candidate. Would the AD5624 be considered a very close replacement for the AD5324? The current DAC is used in a low speed correction loop with an external +5V reference, running at approximately 125kHz sample/update rate. Among the differences I see are pin mapping, and 24-bit DIN vs 16-bit DIN.

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.