Post Go back to editing

High Volgate DAC

Hello,

I am DFAE at Phoenix technologies in Israel.

Nanomotion, one of my customers is interested in DAC with High Output Voltage for motor control application.

Resolution: ≥12bit

Sampling rate: ≥20Ks/s

Output Voltage: ~300V

Analog Multi-channel

They are considering now the AD5535B (32-Channel, 14-Bit DAC with Full-Scale Output Voltage Programmable from 50 V to 200 V), but this solution is 200V maximum output.

Can you recommend about additional solutions for this application?

Maybe soon to be released?

Thanks a lot.

Meir

Parents Reply Children
No Data