The AD5291 datasheet is confusing on the topic of VDD voltage range.  Is it +9 to +33V or +21 to +33V?

The Features section of the datasheet states a VDD voltage range of +9 to +33V, yet the General Description section restricts it to +21 to +33V.  Which is it?

I have a battery powered application where only 15.4V to ~18V are available for VDD [VSS = 0V] {two 9V [7cell] NiMH batteries in series}.  To meet a minimum requirement of +21V would complicate the design.

Can someone with authority please verify the correct VDD voltage range?

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:07 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:07 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data