Hello,
I'm asked AD5666-EP POR function from our customer.
The customer needs DAC which can output midscale after powered on.
And he needs -55 to 125°C temperature range too.
In the datasheet of AD5666 , power-on reset function is described in page-23.
When the POR pin is pulled up , AD5666 output midscale after powered on.
But it is not described about any functions in AD5666-EP datasheet.
Does AD5666-EP have a function to output midscale after powered on ?
The customer wants to confirm it.
Best regards,
ysuzuki