Post Go back to editing

AD5666-EP: POR function

Hello,

I'm asked AD5666-EP POR function from our customer.

The customer needs DAC which can output midscale after powered on.

And he needs -55 to 125°C temperature range too.

In the datasheet of AD5666 , power-on reset function is described in page-23.

When the POR pin is pulled up , AD5666 output midscale after powered on.

But it is not described about any functions in AD5666-EP datasheet.

Does AD5666-EP have a function to output midscale after powered on ?

The customer wants to confirm it.

Best regards,

ysuzuki