AD5412 FAULT PIN SPECS.

What are absolute maximum ratings of FAULT -pin in AD5412?

Is it possible to connect it to +24VDC for example through 2k2 resistor + LED(opto coupler) in serie?

  • 0
    •  Analog Employees 
    on Nov 19, 2015 3:58 PM

    Hi,

    The /FAULT pin is a digital pin so the absolute maximum ratings of the digital output pins to GND is followed.

    To answer your other question, connecting a 24V supply to it will not work and may cause damage to the part.

    If you want to use an opto-coupler, you may connect the /FAULT pin to a 10kΩ pull-up resistor to DVCC. You can send this signal to the opto-coupler. Depending on your current setup, you may have to change supplies if the current is not enough.

    Regards,

    Mark

  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:16 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin