Hello,
I need to generate a 0V to 10V output voltage. Is it possible not connecting AVss Pin? I had planned to connect AVss Pin to gnd but the voltage ranges from -11.4V to -16.5V and I have no negative voltages on my board.
Thanks in advance,
Regards,
MASK-J
Hi MASK-J,
Are you referring to the AD5762R? If so, ADI cannot guarantee that the part will be functional if the AVSS supply requirement is not met. If you wish to work with a DAC that have a single supply operation, you may want to take a look at this pre-selected selection table of ADI's precision DACs. The AD5752R's AVSS can be connected to 0V if the output is unipolar.
Mark
Hi Mark,
Thank you for your answer.