Post Go back to editing

Time chart about AD5302 DAC

Dear Sir/Madam,

 

Our customer tossed the simple question to me.

As for your DAC AD5302 synchronization ,

If the rising edge of /SYNC is placed on the time longer than DB15 to DB0 of DIN, then are your next DB15 to DB0  put(overwrited) on the past DBx?

Otherwise the data that is read by 1st is fixed?

The signal DIN is consecutive signals.

The overwrite is impossible I think correct??

Maybe other DAC will be brought the same motion I believe.....

Please advice this to me!!

Thanks Kaos

  • I just discussed about this with our customer.

    He will also check this motion by one sample AD5302.

    This is very important and need the answer soon.

    So can anyone answer this?

    Thanks Kaos

  • Hi Miguel,

    >Customer bring SYNC low and transfer 16 clocks, right?

    Yes

     

    >SYNC is bring high again sometime later, right?

    Yes,but it needs a long time. It means that t7 is a few seconds eg;.

     

    >there are no extra clocks generated in the SCLK clock between last 16th pulse and SYNC falling edge, right?

    SCLK is still sent in continuously not extra clock generate.

    In other words, is your internal register overwrote after last DB0?

    DB15 to DB0 are sent out continuously from forward circuit.

    Thanks Kaos

  • Hi Kaos,

    Im not fully understand the problem...

    Customer bring SYNC low and transfer 16 clocks, right?

    SYNC is bring high again sometime later, right?

    there are no extra clocks generated in the SCLK clock between last 16th pulse and SYNC falling edge, right?

    Regards,

    Miguel

  • Hi Miguel,

    Here is additional question from customer.

    If /LDAC is fixed to L(connect to GND), then can your AD5302 update the register?

    Your datasheet page-5 said as following.

    "Pulsing LDAC low allows either or both DAC registers to be updated if the input registers have new data."

    Does this mean to need min 20nsec Low pulse?


    Thanks Kaos

     

  • Hi Kaos,

    I guess your question is, when the DAC decodes the command, after the last 16th clock, or bringing SYNC high, right?

    As far as the Ds states,

    1- teh command is decoded bringing SYNC high.

    2- If more than 16th clocks are generated, the part ignores the extra clocks

    If LDAC is pull low, any update on the sift register will be immediately transfer to the DAC register.

    Regards,

    Miguel

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin