What is the max transient voltage/current allowed on Rf during power up. Iout1 is driving into the non-inverting pin of the op amp that is driving it's output back into the Rf pin through a 49.9 ohm resistor. The op amp is powered from ±15. During power up it might be possible to get 14-15 volts on it's output. the Absolute max table shows ±12 as the max. I'm wondering if it changes because of the 49.9 ohms or if there is a time dependence on it.
Ref input is 10V, VDD is 3.3v, and digital inputs are 3.3v signals.
Thanks,
-John