Dear friends. What is the Iout max of DAC AD5445? I cannot find it on Datasheet. Thanks!!
Dear friends. What is the Iout max of DAC AD5445? I cannot find it on Datasheet. Thanks!!
Hi,
The output is designed to be connected to an amplifier and achieve an output voltage. Output could then vary depending on the circuit configuration that will be used.
Regards,
Mark
Dear Mark, thanks for help me.
I want to use the AD5445 'Iout' direct to transistor array LM3046, it will reduce cost in my project once I have port remaining. Iout will be connected to Base of NPN transistor.
I checked the Vout of No-inverting OP and there is no gain config in datasheet. Could I consider same Vout in Iout of Ad5445?
Do you have any suggestion?
Best Regards!
Hi,
When IOUT1 and IOUT2 are kept at the same potential, a constant current flows in each ladder leg, regardless of digital input code. Varying the potential on the IOUT1 would result to unspecified performance of the part. For me to be able to provide a proper suggestion, would you be able to tell more about your application?
Regards,
Mark