Post Go back to editing

AD5421 Power On Reset

Thread Summary

The user asked which pins are latched during the power-on reset of the AD5421. The final answer confirmed that the AD5421 powers on with all registers loaded to default values, and the loop current is set to 3.2 mA or 22.8 mA/24 mA based on the ALARM_CURRENT_DIRECTION pin and selected range. The pins mentioned are input pins that set the part's configuration at power-on.
AI Generated Content

Of the following pins, which ones are "latched" in at time of power-on reset of AD5421?

REG_SEL0

REG_SEL1

REG_SEL2

RANGE0

RANGE1

ACD   

Rint/Rext

Parents Reply Children
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.