Post Go back to editing

AD5421 Power On Reset

Thread Summary

The user asked which pins are latched during the power-on reset of the AD5421. The final answer confirmed that the AD5421 powers on with all registers loaded to default values, and the loop current is set to 3.2 mA or 22.8 mA/24 mA based on the ALARM_CURRENT_DIRECTION pin and selected range. The pins mentioned are input pins that set the part's configuration at power-on.
AI Generated Content

Of the following pins, which ones are "latched" in at time of power-on reset of AD5421?

REG_SEL0

REG_SEL1

REG_SEL2

RANGE0

RANGE1

ACD   

Rint/Rext

Parents
  • Hi,

    The AD5421 powers on with all registers loaded with their default values and with the loop current in the alarm state set to 3.2 mA or 22.8 mA/24 mA (depending on the state of the ALARM_CURRENT_DIRECTION pin and the selected range).

    The most pins that you mentioned are input pins in a sense that the part will power up and will set settings of the part depending on the values of these pins.

    Regards,

    Mark

  • Hi,

     I am Using this AD5421 in 4-20 mA mode.

    Ans I am not able to set current less than 6.5 mA but above 6.5mA i am getting all the values.

    Please let me know what is the issue.

    Thanks 

    Anush

  • Hi Anush,

    Are you using the internal voltage regulator to supply other components? The maximum current that can be drawn from the REGOUT pin should only be 3.15 for you to be able to set the loop current to 4mA. I'm thinking that in your circuit you are drawing 6.5mA from the regulator so you can only set loop currents greater than this value.

    Best regards,

    Rainier

  • Hi,

    Thanks for your reply.

    Yes, Iam using the power from DVCC pin to power up the isolators and the HART modem AD5700.

    As per Current  calculation the total current taken by the isolators ADuM1441 will not exceed 3.15mA.

    I have attached the schematics for you reference.

Reply Children
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.