Post Go back to editing

AD5270 Command Operation

Hello,

Our customer has troubled command operation of AD5270. They send the commands by following order and setting.

   1) 0x2400

   2) 0x1000

   3) 0x1C02

   4) 0x0400

After sending the commands, they checked the position of the digital rheostat wiper. The position was center.

Are there any problems in the order and/or setting of the commands?

And could you please advise me, why do we need an external pull-up resistor on SDO pin if it is not use?

Best regards,

Akira

Parents
  • Hi Akira-san,

    Apologies for the delay.

    My interpretation of the commands are the following:

    1. 0x2400 = device is removed from shutdown mode

    2. 0x1000 = software reset

    3. 0x1C02 = allow update of wiper position through digital interface

    4. 0x0400 = write zero-scale

    From these commands, the expected behavior of the digipot output is at zero scale. Could you try removing the software reset and check if the part is responding? If the part responds, could you check your timing in the SPI lines as you may be violating a specification there.

    Regards,

    Mark

Reply
  • Hi Akira-san,

    Apologies for the delay.

    My interpretation of the commands are the following:

    1. 0x2400 = device is removed from shutdown mode

    2. 0x1000 = software reset

    3. 0x1C02 = allow update of wiper position through digital interface

    4. 0x0400 = write zero-scale

    From these commands, the expected behavior of the digipot output is at zero scale. Could you try removing the software reset and check if the part is responding? If the part responds, could you check your timing in the SPI lines as you may be violating a specification there.

    Regards,

    Mark

Children
No Data