I was reading the datasheet of AD5933, and I did not understand a few things about the calculation for the Rfb value and other things.
This is the Rfb equation:
How do I find the value of Zmin?
I intend to power the AD5933 with 5V, use the 1st Output Range (3Vpp in this case) and PGA gain = 1.
With a frequency sweep of 1K Hz up to 100K Hz:
Internal oscillator: MCLK = 16.776 MHz
fSTART = 1000 Hz
∆f = 1000 Hz
Increments = 99
In addition, I will use a high pass filter with a cutoff frequency of 100Hz, a circuit with a current source controlled by voltage (1mA), and an instrumentation amplifier INA118 (Gain = 2). This circuit will use 4 Electrodes. Similar to this:
In AN-1252 APPLICATION NOTE, page 3 of 12, it is said that for range 1 (Adding external op amp) Zout is equal to "> 100 Ohms". And on page 5, The maximum ratio, ZMAX / ZMIN, for my case is x45. Right? If it is correct. How to calculate Zmax and Zmin for "> 100"?
Furthermore. What is "RCal" for? If I do not use it in any equation.
In the example on page 7, the Zmin value is 4.7K and the Zmax value is 47K. Why? I dont understand.
Hi Kanika,
If you are not using an external AFE, the equation applies as well BUT in teh AN-1252 is explained that the ration between Zmax/Zmin must be lower.
What is your expected Zmin/Zmax range?
Regards,
Miguel
Hi Kanika,
If you are not using an external AFE, the equation applies as well BUT in teh AN-1252 is explained that the ration between Zmax/Zmin must be lower.
What is your expected Zmin/Zmax range?
Regards,
Miguel