how to connetc AD5761

Hi.
I would use "AD 5761" to have a 0-10V output Vout. I have a supply using voltage from 0V to 24V. I only SDI signals SCK and SYNC (as MOSI, SCK and SS of a microcontroller).
I would link /LDAC to Gnd and /CLEAR to Vcc.
This to replace a Max 504 and have an output of 0V to + 10V.
Do you think it can work?

RENATO

Parents
  • Hi Mark.

    I enclose file in .pdf format ad I would link the ad5671.
    I have the microcnotroller inputs at +3.3V.
    I have to obtain an output voltage from 0 to +10V, having available voltages of +24V, +5v and 3,3V.
    I'm not sure I have connected in the circuit diagram the correct voltages.
    You could see if they are correct?
    thanks.
    Best regards
    Renato
Reply
  • Hi Mark.

    I enclose file in .pdf format ad I would link the ad5671.
    I have the microcnotroller inputs at +3.3V.
    I have to obtain an output voltage from 0 to +10V, having available voltages of +24V, +5v and 3,3V.
    I'm not sure I have connected in the circuit diagram the correct voltages.
    You could see if they are correct?
    thanks.
    Best regards
    Renato
Children
No Data