Post Go back to editing

how to connetc AD5761

Hi.
I would use "AD 5761" to have a 0-10V output Vout. I have a supply using voltage from 0V to 24V. I only SDI signals SCK and SYNC (as MOSI, SCK and SS of a microcontroller).
I would link /LDAC to Gnd and /CLEAR to Vcc.
This to replace a Max 504 and have an output of 0V to + 10V.
Do you think it can work?

RENATO

Parents
  • Hi,

    Unfortunately we cannot comment on a competitor's part.

    As for the AD5761, I do not see anything wrong with how you are going to use the part. Would you be able to share what is the application you plan on building? With this knowledge, we can do better recommendation for the selection of the DACs.

    Do you have a working board already? If you are going to use the AD5761, please take note that the part comes in two packages;16-lead LFCSP and 16-lead TSSOP. If you are constrained by any specific package, please share it to us and we will help you look for DACs that would fit you needs.

    I hope this answer your question.

    Regards,

    Mark

Reply
  • Hi,

    Unfortunately we cannot comment on a competitor's part.

    As for the AD5761, I do not see anything wrong with how you are going to use the part. Would you be able to share what is the application you plan on building? With this knowledge, we can do better recommendation for the selection of the DACs.

    Do you have a working board already? If you are going to use the AD5761, please take note that the part comes in two packages;16-lead LFCSP and 16-lead TSSOP. If you are constrained by any specific package, please share it to us and we will help you look for DACs that would fit you needs.

    I hope this answer your question.

    Regards,

    Mark

Children
No Data