I would use "AD 5761" to have a 0-10V output Vout.
I have to obtain an output voltage from 0 to +10V, having available voltages of +24V, +5v and 3,3V.
I have only SDI, SDO, SCK and SYNC signals (as MOSI, MISO, SCK and SS of a microcontroller).
I would link /LDAC to Gnd and /CLEAR to Vcc.
I enclose file in .pdf format ad I would link the ad5671.
I have the microcnotroller inputs at +3.3V.