Post Go back to editing

AD5160 SPI parameters?

Hi,

What would be the correct settings to send data to the AD5160 via SPI. The datasheet tells me that the clock polarity is active low (CPOL = 1) and leading edge triggered (CPHA = 0) regarding the phase. Is this correct?

Thanks in advance!

Kind regards, Samuel Lourenço

Parents
  • Hi,

    An extra question strongly related to this: I need to have this working in SPI mode 3, as I have other devices on the bus, which only works with an inactive high CLK.
    When I look at the datasheet for AD5200, which is somewhat worded similarly in regards to the the interface section, it has a truth table, from which I can see that it would also work fine in SPI mode 3. Unfortnuately, AD5160 lacks this table.

     

    Can you please confirm whether or not the AD5160 will work just a reliably in SPI mode 3 (CPOL=1, CPHA=1) ?

    Thanks

Reply
  • Hi,

    An extra question strongly related to this: I need to have this working in SPI mode 3, as I have other devices on the bus, which only works with an inactive high CLK.
    When I look at the datasheet for AD5200, which is somewhat worded similarly in regards to the the interface section, it has a truth table, from which I can see that it would also work fine in SPI mode 3. Unfortnuately, AD5160 lacks this table.

     

    Can you please confirm whether or not the AD5160 will work just a reliably in SPI mode 3 (CPOL=1, CPHA=1) ?

    Thanks

Children
No Data