AD 5380 eval board

The board is the EVAL-AD5380SDZ. When I load the software, it is able to recognize the board but that's about it - I am not able to change any of the DAC outputs. I am controlling the eval board with an ADI recommended SDP-S board (EVAL-SDP-CS1Z). I also made sure all jumpers were in their default position recommended by the spec sheet. It does not look like the DAC is being programmed at all. I'm using the EVAL-AD5380SDZ and the Analog devices SDPS EVAL-SDP-CS1Z. Can you please suggest a debug process?

Parents
  • Hi rashwin81,

    The EVAL-AD5380SDZ will not work with the SDP-S as it uses the SPORT peripheral which is not present on the SDP-S. You will need to acquire the SDP-B (EVAL-SDP-CB1Z) board to control the AD5380 board as mentioned on the ADDITIONAL EQIUIPMENT NEEDED section on the user guide.

    Best regards,

    Rainier

Reply
  • Hi rashwin81,

    The EVAL-AD5380SDZ will not work with the SDP-S as it uses the SPORT peripheral which is not present on the SDP-S. You will need to acquire the SDP-B (EVAL-SDP-CB1Z) board to control the AD5380 board as mentioned on the ADDITIONAL EQIUIPMENT NEEDED section on the user guide.

    Best regards,

    Rainier

Children
No Data